LTE TDD
This topic describes carrier settings for Real-Time capability.
All carrier settings are read-only when the real-time carrier state is on because only one real-time carrier is available for this release (A.14.00).
Wherever <carrier> appears in the SCPI command descriptions of this topic, that value is fixed to 1 for this release (A.14.00).
<carrier> is constructed from Carrier ID and Carrier Type.
Special Subframe Configuration
Displays the enable state of a carrier.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>[:STATe]? |
SCPI Example |
RADio:LTET:WAVeform:RTIM:CCAR? |
Notes |
Query only |
State Saved |
Yes |
Preset |
ON |
Initial S/W Revision |
A.14.00 |
This setting returns the carrier type. This setting is automatically set when a carrier is added.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:TYPE? |
SCPI Example |
:RAD:LTET:WAV:RTIM:CCAR:TYPE? |
Notes |
SCPI only, Query only Returns TDDULEUTRA |
State Saved |
No |
Preset |
TDDULEUTRA |
Range |
Uplink E-UTRA |
Initial S/W Revision |
A.14.00 |
This node is available when a TDD carrier is selected.
Sets the uplink-downlink configuration.
The supported uplink-downlink configurations are defined in Table 4.2-2 of 3GPP TS 36.211.
Coupling: For Basic, Advanced UL, and Advanced DL LTE-A TDD when Auto Carrier Aggregation Configuration is set to On, this setting is read only for the secondary cells that has the same value as the primary cell.
The resource blocks and some parameters are reconfigured by changing the Uplink Downlink Configuration parameter in the same manner as Predefined Configuration.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:UDConfig <integer> [:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:UDConfig? |
SCPI Example |
:RAD:LTET:WAV::RTIM:CCAR:UDC 2 :RAD:LTET:WAV::RTIM:CCAR:UDC? |
State Saved |
Yes |
Preset |
0 |
Min |
0 |
Max |
6 |
Initial S/W Revision |
A.14.00 |
Displays the Switch-point periodicity of the frame. Refer to Uplink-downlink allocations in 3GPP TS 36.211 Table 4.2-2.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:SPPeriodicity? |
SCPI Example |
:RAD:LTET:WAV::RTIM:CCAR:SPP? |
Notes |
Query only Returns <time> Unit in GUI: s Range: 5 ms, 10 ms |
State Saved |
No |
Preset |
5 ms |
Min |
5 ms |
Max |
10 ms |
Initial S/W Revision |
A.14.00 |
Display Downlink/Uplink Allocation Configuration. Refer to Uplink-downlink allocations (Table 2) in 3GPP TS 36.211.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ACONfig? |
SCPI Example |
:RAD:LTET:WAV::RTIM:CCAR:ACON? |
Notes |
Query only Return <string> ex: "D,S,U,U,U,D,S,U,U,U" |
State Saved |
No |
Preset |
"D,S,U,U,U,D,S,U,U,U" |
Initial S/W Revision |
A.14.00 |
Sets a special subframe configuration.
If corresponding Component Carrier is set to secondary cell and Auto Carrier Aggregation Configuration parameter is set to On, Special Subframe Configuration is set same as the primary cell value and set read only.
See 3GPP TS 36.211 section 4.2 for more information.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:SSFRame:CONFig <integer> [:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:SSFRame:CONFig? |
SCPI Example |
:RAD:LTET:WAV:RTIM:CCAR:SSFR:CONF 1 :RAD:LTET:WAV:RTIM:CCAR:SSFR:CONF? |
Dependency |
Cyclic Prefix |
State Saved |
Yes |
Preset |
0 |
Min |
0 |
Max |
9 (for Normal Cyclic Prefix) 7 (for Extended Cyclic Prefix) |
Initial S/W Revision |
A.14.00 |
Displays the symbol length of DwPTS. See Table 4.2-1 (with X = 0) in 3GPP TS 36.211 for details.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:DPTS:SYMBols? |
SCPI Example |
:RAD:LTET:WAV:RTIM:CCAR:DPTS:SYMB? |
Notes |
Query only GUI label: DwPTS Length (symbol) |
State Saved |
No |
Preset |
3 |
Initial S/W Revision |
A.14.00 |
Displays the symbol length of GP.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:GP:SYMBols? |
SCPI Example |
:RAD:LTET:WAV:RTIM:CCAR:GP:SYMB? |
Notes |
Query only GUI label: GP Length (symbol) |
State Saved |
No |
Preset |
10 |
Initial S/W Revision |
A.14.00 |
Displays the symbol length of UpPTS.
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:UPTS:SYMBols? |
SCPI Example |
:RAD:LTET:WAV:RTIM:CCAR:UPTS:SYMB? |
Notes |
Query only GUI label: UpPTS Length (symbol) |
State Saved |
No |
Preset |
1 |
Initial S/W Revision |
A.14.00 |
The buttons of carrier configuration tools may appear when a carrier is configured. Refer to specific carrier sections for more details of the carrier configuration buttons. The configuration buttons are configured differently by each carrier.